Valves to be used in system with 28% bio-ethanol.

Issue

Are the V211T, V222, V292 valves suitable in a system containing 28% bio ethanol?

Product Line

Field Devices

Environment

  • V211T
  • V222
  • V292

Cause

Application requirement on content.

Resolution

With a content of only 28%, the valves should work just fine. Cast iron is not ideal, but it works fine. Stem packing materials are EPDM and teflon, and they will also work fine with this content.