What card is needed to attach the DX8100HDDI to the DX8100 Series HVR?

Issue

What card is needed to attach the DX8100HDDI to the DX8100 Series HVR?

Product Line

Pelco Video Management

Environment

  • DX8100HDDI
  • DX8100

Cause

DX8100HDDI needs SCSI interface card to connect to DX8100.

Resolution

The card to attach the DX8100HDDI to the DX8100 is DX8100-ISCI.

Note: The SCSI card will be installed in slot 5 on the DX8100 PCI Express, the cable connection type is VHDCI to VHDCI SCSI round cable type.

DX8100HDDI Install Manual