What are the model numbers for the Network Interface Cards installed within the DSSRV?

Issue

DSSRV unit is unable to connect to the Local Area Network.

Product Line

Pelco Video Management

Environment

  • DSSRV only
    • Does not include the DSSRV2 series

Cause

Corrupt NIC card drivers installed on the DSSRV unit.

Resolution

Network Interface Card models installed on the DSSRV unit include:

  1. Intel(R) 82579LM Gigabit Network Connection
  2. Intel(R) 82583V Gigabit Network Connection

NIC cards are integrated into the motherboard and are not a sperate item that can be repaired.

Note: These are not part numbers that you can order.