Pelco Media Player v1.9.x will not work with Internet Explorer 11 (IE11) unless in Compatibility Mode

Issue

Pelco Media Player v1.9.x will not work with IE 11 unless Compatibility Mode is enabled.

Product Line

Pelco Cameras

Environment

  • Pelco Sarix series IP cameras
  • Pelco Media Player v1.9.x
  • IE11

Cause

64-bit IE11 cannot run the 32-bit activex control.

Resolution

Use the Pelco Media Player in Compatibility Mode in Internet Explorer.

Related information:
Why is Pelco Media Player recommended over Quick Time?
Where can I download the Pelco Media Player?
Pelco Media Player compatible web browsers

Pelco Media Player v1.9.5.1.zip