If using the IPV6 address the PTZ controls will not work with the web UI

Issue

The Web UI cannot PTZ Sarix cameras if using an IPV6 address scheme.

Product Line

Pelco Cameras, Pelco Video Management

Environment

When using IPV6 addressing and trying to PTZ using the web UI

Cause

Firmware issue, may be fixed in a future release

Resolution

There is no current work around other than using IPV4 addressing