Channel numbers for 1+5, 1+12 and 2+8 screen layouts for Endura scripts

Issue

Which channel numbers do i have to use in the 1+5,1+12 and 2+8 screen layouts?

Product Line

Pelco Monitors, Pelco Video Management

Environment

Endura WS5200,VCD5200 and NET5402R-HD

Cause

Channel id numbers of the 1+5,1+12 and 2+8 screen layouts?

Resolution

When you want to use Endura's scripts to occupy a certain place of a multiplexed layout on a monitor you have to use channel numbering within the script.
However with the 1+5, 1+12 and 2+8 layouts the counting is a bit different than normal left to right, in the following images are the channel numbers displayed for these layouts:

1+5 Layout     1+12 Layout     2+8 Layout