WARNING
ELECTROSTATIC DISCHARGE REQUIRED.Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.
Issue
Need to know how to use the AUX2 on the Esprit ES40/41
Product Line
Pelco Cameras
Environment
Pelco Esprit ES40/ES41 Series Positioning System
Pelco Esprit ES30/ES31 Series Positioning System
Cause
Aux-2 specifications
Resolution
An open collector output is the same as an electronic switch has only open and close functionality and do not providing any voltages to the external accessory device.
For the Esprit:
Important note:
The external accessory device must not exceed 40mA and 32VDC to trigger the relay coil.