How to wire up the PS20-24 scanner without the controller.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

How do I wire the PS20-24 Scanner without a controller?

Product Line

Other, Pelco Cameras

Environment

  • PS20
  • PS20-24
  • Wiring without controller

     

    

Cause

Wiring option for PS20 Scanner without controller. Continuous scan.

Resolution