NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
Why does Pelco NET manager show NET300R as a transmitter and not receiver?
Product Line
Pelco Transmission & Power
Environment
- NET300R
- NET300T
- NET350T
- NET350R
- NET Manager.
Cause
Net manager software displaying NET300R or NET350R as a transmitter device.
Resolution
The Net-Manager program detects the NET300R/NET350R as transmitters. The netmanager discovery code was originally designed for detection of Pelconet NET100T as transmitters and NET100R as receivers.
Determine NET300R or NET350R by either of two options:
- Browser page connection.
- MAC Address as labeled on the NET receiver encoder.
Note: NET300/NET350 series do not feature DHCP option. An IP addressed is manually assigned.