What SCSI card is used on a legacy (Integral) Digital Sentry DVR.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

The DS Xpress is not booting up with a new SCSI card installed.

Product Line

Pelco Video Management

Environment

  • DS XPress
  • DS 1000
  • DS RealVue XPress

Cause

  1. Wrong SCSI card installed.
  2. The BIOS in the SCSI card may need to be disable.

Resolution

Install the correct SCSI card which matches assembly date.
 

Units assembled in 2006 or earlier:

  • 6750-00007 (Adaptec 2916LP) 
     

Units assembled in 2009 - 2007:

  • 6750-00011 (Adaptec 29320LPE)  - DVRs using the Super Micro Mother Board