How to Virtual PTZ a Oncam Grandeye IP camera on a DS Control Point.

Issue

PTZ an Oncam Grandeye EVO using Controlpoint.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry (version 7.5.609 and higher)
  • DS Control Point Software (version 7.5.609 or higher)
  • Oncam Grandeye 360
    • EVO Series all models

Cause

Virtual PTZ information on Oncam Grandeye.

Resolution

 To view and virtual PTZ Oncam Grandeye 360 camera

Option 1:

  1. Left click and hold Grandeye camera and drag and drop in layout display.
  2. Enable on screen PTZ (turns green); then select the Jotstick icon which will display the PTZ control menu.


     
  3. Click on the arrow icon to move viewing location.
  4. Click Zoom + or Zoom- for a close or far view.


     

Option 2:

  1. Click on the Grandeye virtual PTZ icon and use the mouse on the image to ptz by using the left mouse button for PTZ and mouse wheel for zoom.