NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
The DS Xpress is not booting up with a new SCSI card installed.
Product Line
Pelco Video Management
Environment
- DS Xpress
- DS RealVue Xpress
- DS1000
Cause
Boot process using the external storage SCSI card instead of the internal OS drive.
Resolution
NOTE: SCSI cards affected
6750-00007 (Adaptec 29160LP) for units build on 2006 or older.
6750-00000 (Adaptec 29320LPE) for units build on 2007 or newer including DSSRVs.
Steps to disable BIOS in the SCSI card:
- Upon boot up press CTRL-A when prompt.
- Press the ENTER key.
- Press the ENTER key again.
- Select Advance Configuration.
- Press the ENTER key.
- Change SCSI Controller Int 13 from Enable to Disable: Scan Bus.
- Press Esc key two times.
- Select Y to save the changes.