Is it possible to use an Automation Server as a LON Device in an OpenLNS Database using the OpenLNS Commissioning Tool?

Issue

Is it possible to use an Automation Server as a LON Device in an OpenLNS Database using the OpenLNS Commissioning Tool?

Product Line

SmartStruxure Solution

Environment

Automation Server 1.4.1.68 or newer

External Lonworks network, not managed via Automation Server/Workstation

Cause

Some sites may wish to use other Lonworks configuration tools than StruxureWare Building Operation Workstation

Resolution

This is possible in 1.4.1.68 and newer. Add a Lonworks Local FT-10 interface and then add an Externally Managed Lonworks Network.