KBD300A CODE 57 or 52

Issue

When powered up KBD300A shows 57 on led or 52

Product Line

Pelco Video Management

Environment

  1. KBD300A Version 5.70
  2. KBD300A Version 5.20

Cause

  • Powering up KBD300A
  • KBD300A LED display flash a two digit number.

Resolution

The KBD300A will flash a sequence of numbers for the red led display when power is applied. The display is intended to indicate the firmware version of the keyboard.

example: The numbers 57 flashing indicate the KBD300A is running firmware version 5.7.  Earlier versions will flash numbers such as 51 or lower.
 

 

View the related Lessons Learned articles by clicking on the title below: