What are the valid ACCNet ID ranges for Controllers and Cyberstations?

Issue

How many controllers and Workstations can Continuum systems support?

Product Line

Andover Continuum

Environment

All Ethernet level controllers and Workstations.

bCX, CX, NCII, ACX

Cause

Valid address ranges required

Resolution

Each "Network" (often called Continuum Network or Infinity Network) supports controllers with ACCNetID values of 1 to 190.

No duplicate numbers are allowed on the same network

Potentially the database supports up to 4 Million networks.

Cyberstation workstations have ACCNetID's in the range 191 through 254 (maximum 64)