CM9700-CC1 CPU controllers A drive not reading the floppy disk.

Issue

Floppy disk drive will not read the floppy disk.

Product Line

Pelco Matrix

Environment

  • CM9740-CC1 all versions
  • CM9760-CC1 all versions
  • CM9700-CC1 all versions

     

Cause

Floppy disk drive is possible dirty.

Resolution

Use compressed air to blow the dirt out of the floppy drive and try again.