If I add a TAC Xenta to an existing TAC Xenta group, do I have to update other Xentas as well?

Issue

If I add a TAC Xenta to an existing TAC Xenta group, do I have to update other Xentas as well?

Product Line

TAC Vista

Environment

  • TAC Xenta programmable controller
  • Xenta groups
  • Vista system plugin

Cause

Each time a group member is added, the whole group needs to be downloaded. This provides new network description files to the controllers so they communicate properly.

Resolution

All Xentas in that group must be updated. LonMaker and your Vista databases need to be updated as well.