Language pack installation have no effect.

Issue

Installed language pack on PC but the language doesn't change

Product Line

SmartStruxure Solution

Environment

SmartStruxure Workstation

Cause

The operating system language of the computer on which WorkStation is installed determines the language that WorkStation displays in. For example, if the language of an operating system is Spanish, WorkStation is displayed in Spanish, provided that the Spanish language packages are installed

Resolution

You have to have the same language on the Operating system as the Language pack.