Changing a Controlli MVL56C actuator with an SE Forta actuator when fitted to an VMB16 - 125 Controlli valve.

Issue

Changing a Controlli MVL56C actuator.

Product Line

Field Devices

Environment

MVL56C

VMB

VMB16

Cause

A Controlli MVL56C actuator is to be replaced, is a linkage required to connect to a Forta actuator?

Resolution

A linkage is required.

The linkage is the AG50, part number 880-0127-000