Not able to change IP camera name with Russian characters on DS Version 7.5.609.8802

Issue

Digital Sentry version 7.5.609.8802 is not able to change IP camera name in Russian characters and get an error.

Product Line

Pelco Video Management

Environment

DSSRV - Version 7.5.609.8802

DSNVS - Version 7.5.609.8802

Cause

Programming custom camera name/titles for the system.

Resolution

As workaround do not use the General tab to change the IP camera name in Russian characters, but click on

the 'On Screen Display' tab to change the camera name in Russian characters then click the save button.