Will the KBD300A do coaxitron control?

Issue

Need to replace a MPT9500 Coaxitron Keyboard.

Product Line

Pelco Cameras, Pelco Monitors, Pelco Matrix, Pelco Transmission & Power

Environment

KBD300A Universal Keyboard all versions

Cause

No data wires available to the camera.

Resolution

No, the KBD300A will not do coaxitron control, in direct mode it will do "P" protocol at 4800

baud rate and no parity (none) or "D" protocol at 2400 baud rate and no parity (none). For

coaxitron control will require a coaxitron matrix such as the CM6700-MXB2(4).