How to remove the on screen text display from EHXM30 series?

Issue

How to get rid of the on screen text display coming from EHXM30 series.

Product Line

Pelco Cameras

Environment

  • EHXM3036
  • EHXM3136
  • EHXM30C22
  • KBDKIT
  • KBD300A

Cause

On Screen text display is blocking video image.

Resolution

  1. Set dip switch on KBD300A to P or D protocol refer to keyboard manual page 26 of  C527M-L (3/04).
  2. Set dip switch on EHXM30 match KBD300A protocol D1/2400 or P1/4800.
  3. Connect data control wires from EHXM30 RX+/RX- will land on KBDKIT TX+/TX-.
  4. Once connection it done using KBD300A controller do Zoom function display text on screen will clear out.