Is there a cross-reference or functional replacement for the ENC-520-2 or ENC-410-1?

Issue

Customer Care cannot offer a cross-reference or functional replacement to a caller looking to order an ENC-520-2 or ENC-410-1 which are obsolete.  Does one exist?

Product Line

TAC I/A Series

Environment

Niagara G3

Cause

Product obsolescence

Resolution

Depending on the jobsite's network architecture and protocol integrations, the functional replacement to an ENC-520-2 or ENC-410-1 can vary. 

Contact your Regional Sales Manager for assistance in selecting the correct replacement part.