Do I need to install Endura Mapping on both the primary and secondary system manager?

Issue

The customer has both a primary and secondary system manager. They also have installed mapping onto the primary system manager using the mapping system installer. Do they need to repeat the process for the secondary SM5000?

Product Line

Pelco Video Management

Environment

Endura SM5000 system manager, all versions

Cause

Failover replication does not replicate the mapping program.

Resolution

Yes.  The Endura Mapping System Installer must be pointed to both the primary and secondary system manager.  In the event that a system manager undergoes a failover, the mapping services will not be impacted.