Database update error Installation Error! Microsoft ODBC SQL Server Driver SQL Server]Implicit conversion from data type datetime to int is not allowed. Use the CONVERT function to run this query. Updating 1.94 to 1.94 SP1

Issue

An update from 1.94 to 1.94 SP1 will generate an Installation error Microsoft ODBC SQL Server Driver SQL Server Implicit conversion from data type datetime to int is not allowed

Product Line

Andover Continuum

Environment

Continuum

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

A column in the db doesn't get converted properly SQL Server Implicit conversion from data type datetime to int is not allowed Use the CONVERT function to run this query

Resolution

To correct this issue apply the following hotfix AFTER installing 1.94 SP1 but BEFORE running the database update

Hotfix for DataBase Update Error