Issue
How many trendlogs can the Xenta 511 handle? How many log values can be stored?
Product Line
TAC Vista
Environment
Xenta 511
Cause
Knowing limitations on the maximum number of trends and trend data helps engineer the system properly.
Resolution
150 trendlogs are supported. Total 100,000 values are possible to store.