Which valve to use with the MZ140 actuator?

Issue

When replacing a valve where the MZ140 actuator is used, which valve will fit?

Product Line

Field Devices

Environment

MZ140-24T

MZ140-230T

VZ208E, VZ308E, VZ408E
VZ208C, VZ308C, VZ408C

Cause

Valve that fits the MZ140 actuator

Resolution

The MZ140 is designed to be used with the VZ*08* valves (VZ208E, VZ308E, VZ408E
VZ208C, VZ308C, VZ408C).