Display PDFs in webpinpoint

Issue

There is a need to be able to display pdf files from within a webpinpoint graphic

Product Line

Andover Continuum

Environment

Webclient

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

instructions to open a pdf file with webpinpoint

Resolution

Within a graphic in Cyber Pinpoint, add a Windows Control> Web Browser object

Edit the object and go to object properties and select the .pdf to display (Change the file type drop down to all files from .htm) 

It is recommended to place the pdf files in C:\program files\Continuum\NewGraphicsFiles for permissions reasons. 

Once that object has been selected, it can be saved and run in Cyber Pinpoint The same object will open up webpinpoint and the pdf will display.