What is the part number for the rack mount kit on the DSSRV recorder or Endura SM5200?

Issue

Would like to order a new rack mount kit for DSSRV recorder or Endura SM5200

Product Line

Pelco Video Management

Environment

  • DSSRV
  • DSSRV2
  • DS-CPPC
  • NSM5200
  • WS5080
  • SM5200 RACK MOUNT KIT
  • DSSRV KIT
  • DSSRV Rack Ears

Cause

The original mount kit is broken or missing.

Resolution

The Rack Ears ZSPDSSRV-0003 (2 qty)

The rack mount kit part number ZSPDSSRV-0002 includes:

  • Sliding Mounting Brackets.(2 qty)
  • Front L shaped brackets(2 qty)
  • Rear L shaped brackets (2 qty)
  • L shaped plate nut (4 qty)
  • M5*8L-H2.5 Round Head Nickel Screws (18 qty)
  • M4*6L-H2.5 Round Head Nickel Screws (18 qty) 
  • 4.2*11*0.8 Nickel Washers (10 qty)

  



 

Note:
The unit can be mounted in an industry standard 48 cm (19-inch) equipment rack and occupies 2 rack units (RU) of vertical rack space (8.9 cm or3.5 inches). Minimum distance from front and back verticle mounting rails in rack is 19.5 inches for our rails.