DANGER
HAZARD OF ELECTRIC SHOCK.Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.
WARNING
ELECTROSTATIC DISCHARGE REQUIRED.Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.
NOTICE
POTENTIAL FOR DATA LOSS.The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.
Issue
UDI5000-MTRX not responsive when connecting serial device to DB9 serial port
Product Line
Pelco Video Management, Pelco Matrix
Environment
- UDI5000-MTRX: Rev A1 (New Hardware)
Cause
The UDI5000-MTRX serial port is non-operational due to a connection issue during assembly.
Resolution
The following steps must be performed for the serial port of the UDI5000-MTRX to work.
1. Power off the UDI5000-MTRX and remove the top covers screws and cover.
2. You should see the following if the serial ribbon cable is connected incorrectly to the serial port motherboard header.
3. Pull the connector straight up and flip 180 degrees, reconnect to the serial port header. It should look like the picture below.
4. Reinstall the top cover and screws.