ESTI Series Switches for Pan, Tilt, and Zoom (PTZ) Control.

Issue

Set thermal cameras for RS-422/485 operation.

Product Line

Pelco Cameras

Environment

  • ESTI314-2/5 models
  • ESTI335-2/5 models
  • ESTI350-2/5 models
  • ESTI3100-2/5 models
  • ESTI635-2/5 models
  • ESTI650-2/5 models
  • ESTI6100-2/5 models

Cause

  • Installation

Resolution

Switch Locations, definitions, and settings can be viewed per the installation manual or via link provided below.

View switch settings table here: Switch Settings Table

To access the DIP switches:

a. Remove the plug from the left cover of the pan/tilt. It is not necessary to remove the pan/tilt cover.

b. Set the baud rate (SW1) and receiver address (SW2).

c. Replace the plug