How to install the Oncam Grandeye 360 Evolution indoor IP camera.

Issue

How to mount the Oncam Grandeye 360 Evolution indoor IP camera.

Product Line

Pelco Cameras

Environment

  • Oncam Grandeye 360 Evolution
  • EVO Series all models

Cause

  • Lost the template for the drill holes of the indoor mount.
  • Lost the Quick Install Guide.

Resolution

To download the drill hole template of the Oncam Grandeye 360 Evolution camera click here.

To download the Quick Install Guide click here. (may need to rotate picture clockwise, to do this right - click the mouse and click rotate)