Modbus extended register

Issue

Need more than 50000 registers in a modbus device

Product Line

SmartStruxure Solution

Environment

SmartStruxure

Cause

The Modbus specification sets a limit of 65535 as the largest register number.

Resolution

Enter the value into the Register number configuration property. The Modbus specification sets a limit of 65535 as the largest register number.