TXB-IP Preset 95

Issue

Enter the Preset 95 menu on Cameras using Atlas based firmware.

Product Line

Pelco Cameras

Environment

  • TXB-IP
  • Atlas Firmware all versions.
  • Spectra IV IP
  • Spectra Mini IP
  • IP110
  • IP3701

Cause

  • Installation and Configuration.
  • Analog Programming features.
  • Exiting preset 95 menu

Resolution

Using a Web browser; login to the camera.

 

 

 

Exit preset 95 menu

  1. Click on the "PTZ Display" if not open.
  2. Navagate to "Exit" 
  3. Select "Iris open"