Sarix IMP319 series relay handler repeats itself with sabotage alarm

Issue

Relay handler triggers however there is no reason any more to trigger

Product Line

Pelco Cameras

Environment

Sarix IMP319 series 

Cause

During the setup of a relay contact which will trigger on a  camera sabotage alarm you enable the sabotage first and after that you configured and enabled the handler (relay).

Resolution

First configure and enable the relay handler and afterwards enabled the sabotage to have this option work properly without repeating itself.