Spectra HD Imaging Settings General Tab

Issue

Where to adjust camera image settings of Spectra HD

Product Line

Pelco Cameras

Environment

  • SD5330

Cause

Adjusting Focus

Resolution

 

Use the Imaging tab to change the camera's general image settings, adjust the camera exposure, tune the white balance settings for scenes with fluctuating lighting conditions, define window blanking privacy areas, configure presets and preset tours, and select positioning settings.


Click on any of the following images for view of definition and considerations to image changing: