Wiring details when connecting an ARA 659 Esbe actuator to a Satchwell CZT 5305 controller.

Issue

Connecting an ARA 659 Esbe actuator to a Satchwell  CZT 5305 controller.

Product Line

Field Devices

Environment

Esbe

ARA 659

ARA 600 Series

Wiring

Cause

Confirmation of the actuator wiring connections to the controller.

Resolution

The actuator is connected as follows;

CZT 5305 - Esbe ARA 659 actuator.

Terminal 36/37 - 24 volts (Brown wire).

Terminal 35 - 0 volts (Blue wire).

Terminal 19 - 0-10 volt (Black wire).- Heating actuator.

Terminal 20 - 0-10 volt (Black wire).- Cooling actuator.

To review the CZT 5305 datasheet please click HERE.

To review the ARA 600 series datasheet please click HERE.