Pelco Oncam Grandeye Evolution 360 Information and Specifications

Issue

Pelco Oncam Grandeye Evolution 360 Information and Specifications

Product Line

Pelco Video Management

Environment

  • Oncam Grandeye Evolution 360
    • Evolution 05 v1.9.11 or higher require VLC Plugin
    • Evolution 05 Mini v1.9.11L or higher require VLC Plugin 
    • Evolution 12 v1.1.49  or higher require VLC Plugin 
  • DigitalSENTRY Series
  • DSSRV
  • DSSRV2

Cause

Specifications and general information for configuration of the Oncam Grandeye Evolution for use with DigitalSENTRY Series products.

Resolution

Motion Recording
DSSRV supports up to 6 Oncam EVO-05 / EVO-12 cameras
DSSRV 2 Supports up to 8 Oncam EVO-05 / EVO-12 cameras
 
Continuous Recording
DSSRV supports up to 8 Oncam EVO-05 / EVO-12 cameras
DSSRV 2 Supports up to 8 Oncam EVO-05 / EVO-12 cameras
 
Keep in mind that all firmware updates will be provided by Oncam Grandeye. Below you will find links to the information available at the Oncam Grandeye website:

Source: Pelco Panoramic IP Cameras Evolution 360 Product Page

Oncam Grandeye Website

Oncam Grandeye Support Site 
*Note that in order to download the firmware/software you will need to create an account.

In addition to the contact information, the camera information will be different. The default IP settings will be the Oncam Grandeye defaults. Below you will find the default information for the Oncam Grandeye Evolution 360:

Default Username: admin
Default Password: admin
Default IP: 192.168.0.200
DHCP: On By Default

 

Also available is the camera viewer. This tool will allow you to connect directly to the Oncam Grandeye Evolution 360 camera and verify that live video is being received and that dewarping is working. That tool is available from the link below:

Oncam 360 Viewer

The Oncam configuration tool, this is equivalent to Device Utility. It will allow you to discover Oncam cameras on the network and set IP addresses, as well as change the admin password.

Oncam Configuration Tool
*
Note if the password for the camera is forgotten this will require a camera reset. Please see the manual for the procedure for resetting the camera.

Unavailable Features

The alarm contacts can be triggered on the camera using the motion interface but there is no way to include that programming into DS and it is not planned for integration.
No Dewarping (PTZ) when Viewing Oncam on Pelco mobile.

Troubleshooting

If you are having problems adding an Oncam Grandeye Evolution 360 to DigitalSENTRY, please see the following article for assistance in running DS QuickSetup

No "Grandeye configuration tab" in DS Quicksetup

Related Articles:
How to add and configure a Oncam Grandeye EVO-05 to a Digital Sentry (DSSRV) recorder.
Does the Oncam Grandeye Evolution 360 (EVO-05) support "In-Camera" motion detection?