DX8000 Live Video Clips.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

The Live video framerate can be adjusted in the DX8000 Software

Product Line

Pelco Video Management

Environment

  • DX8000 Software versions below 2.0

Cause

  • Framerates below 15 FPS clip video.

Resolution

To access the Frame Rate Configuration dialog box:

  1.  On the DX8000 toolbar, click SETUP. The Setup dialog box opens to the Camera page.
  2.  In the Setup dialog box, click SCHEDULE . The Schedule page is displayed.
  3.  In the Camera Settings section, click Frame Rate Configuration. The Frame Rate Configuration dialog box opens.

These settings configure the frame rates. To adjust the resolution click on advanced.