What size microSDHC card does the IPCT01 IP Camera Installation Tool support?

Issue

What size microSDHC card does the IPCT01 IP Camera Installation Tool support?

Product Line

Pelco Cameras

Environment

  • IPCT01

Cause

What are the different microSDHC card sizes that are supported by the IPCT01 IP Camera Installation Tool?

Resolution

The IPCT01 IP Camera Installation Tool supports the following microSDHC card sizes.

  • 2GB
  • 4GB
  • 8GB
  • 16GB
  • 32GB

 

More information regarding the IPCT01 IP Camera Installation Tool can be located here.