No live video from Openeye NE-VS201 IP Video Encoder connected to the DSSRV utilizing ONVIF driver

Issue

No live video from Openeye NE-VS201 IP Video Encoder connected to the DSSRV utilizing ONVIF driver

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • DSSRV
  • DSNVR
  • DSNVS

Cause

Openeye NE-VS201 IP Video Encoder does not support ONVIF profile S or version 1.02. ONVIF support for the Openeye NE-VS201 IP Video Encoder limited to version 1.01

Resolution

 Manually add the Openeye NE-VS201 IP Video Encoder to the Digital Sentry VMS via DS Admin utilizing RTSP streams

  1. Add Openeye NE-VS201 IP Video Encoder selecting “other” as the driver to allow for the addition of the RTSP stream URL
  2. Configure video parameters of the Openeye NE-VS201 IP Video Encoder utilizing max IPS, max resolution and H.264 compression type.
  3. Add username of “Admin” and password of “1234”
    • Default username and password for the Openeye NE-VS201 IP Video Encoder
  4. Enter the IP Address of the Openeye NE-VS201 IP Video Encoder
    • Do not change the default Input on IP Device from one.
  5. Enter the RTSP stream URL rtsp:///h264
  6.  Click OK
  7. Verify live video via On-Screen Display tab of DS Admin
    • Note: Additional RTSP stream URL
      • rtsp:///jpeg
      • rtsp:///mpeg4
      • rtsp:///h264 - Stream 1
      • rtsp:///h264_2 - Stream 2
      • rtsp:///h264_3 - Stream 3
      • http://:8008