How to have visibility into what a controller sees in its list of peer controllers and Cyberstations following a teach.

Issue

How to have visibility into what a controller sees in its list of peer controllers and Cyberstations following a tech.

Product Line

Andover Continuum

Environment

All CX controllers

Cause

Documentation

Resolution

If controller is 9900 you can perform a 'dump controller" from Hyper Terminal and see the list of peer controllers and CyberStations the controller has been taught.

For Second Generation Continuum controllers that do not have a terminal interface you can put a program in the controller to get information about the list.

(you can use the program in the 9900 as well)

Click HERE to see a sample PE program.

IMPORTANT UPDATE:

If the site has more than just a few (3-5) controllers comment out the line in the program that gets the controller names.

Also, comment out the line that gets the security flag if there are first generation (9900, 9640) controllers involved.