Where can standard graphics and snippets be found?

Issue

Example graphics components required

Product Line

SmartStruxure Solution

Environment

TGML - Building Operation Graphics Editor

Cause

No standard graphics or components are supplied within the product.

Resolution

A Standard graphic component library can be downloaded from the Buildings Download Center.

This consists of a number of Component Libraries that can be installed on a Workstation by double clicking on each one.

In your TGML Editor, Right click in the Components window and select "Categories" you can then select the categories you require to see in your components section.

There are also a lot of standard Snippets that have been developed by users around the world, these are available to download from the Buildings Business Community site (Search for Snippet Library).