Digital Sentry 2.2 - 4.1 default SQL SA password

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What is the default 'sa' SQL account password for DS installations using software version 2.2 or 4.1?

Product Line

Pelco Video Management

Environment

  • Digital Sentry version 2.2 - 3.0.1.1 - 4.1
  • DS XPress
  • DS Enterprise
  • DS RealVue

Cause

User accounts failing authentication and the "Rebuild Users" script is not correcting, access to the database is required using SSMSE.

Resolution

Default 'sa' password = dsserviceuser

Note: There is the option to change the default password when installing the software so the above default is not guaranteed to work.