With the availability of TreeTech 3.2, can the version embedded with InVue be upgraded?

Issue

Site has InVue with embedded TreeTech version 1.1.  Now that a newer version of TreeTech is available (version 3.2), can version 1.1 be upgraded?

Product Line

TAC I/A Series

Environment

InVue

Wonderware for Intelligent Buildings (WIB)

TreeTech

Cause

Product upgrade question

Resolution

TreeTech version 3.2 is not compatible with InVue.  TreeTech version 1.1 is the only compatible version with InVue.

TreeTech version 3.2 is designed to run 'stand-alone'.  It is not designed to run with any other software package.
It is used to backup GCM databases.