Issue
How to record motion detection video to the SD card on a Sarix.
Product Line
Pelco Cameras
Environment
Sarix Professional Series
- IMP - Mini Dome Cameras
- IBP - Bullet Cameras
- IXP - Box Cameras
- MicroSDHC or MicroSDXC 32GB cards (Provided by customer)
Cause
Sales or Setup information on Sarix Professional Series.
Resolution
- To setup motion record to a SD card Login to the Sarix Professional Series. (User/Password:admin)
-
Navigate to the Event menu and Select from the drop down menu "SD Recorder Handler"
- Click the SD Format icon. NOTE: The SD card must be formatted as FAT32. Other formats are not compatible with the camera.
- Enable "SD Record Handler"
- Select "Motion Detection" for Trigger.
- Select "Time interval" (5 or 10 seconds)
- Select On or Off for video over write.
-
Save when done.
- Navigate to the Event menu and Select from the drop down menu "Motion Detection"
- Enable "Motion Detection"
- Set the desired area to trigger motion detection in the Live Preview window.
-
Save when done.
Related Articles:
How to playback video recorded to an SD card on the Sarix Professional series cameras.