Can the PMCL419 Reset to defaults

Issue

Factory reset procedure

Product Line

Pelco Monitors

Environment

  • PMCL415 - 15-inch (381 mm) active TFT LCD monitor
  • PMCL417 - 17-inch (432 mm) active TFT LCD monitor
  • PMCL419 - 19-inch (483 mm) active TFT LCD monitor

Cause

  • Service

Resolution

NOTE: There is no reset feature to return the monitor to factory defaults.