USB port on STD300

Issue

What is the USB port used for in the STD300?

Product Line

Field Devices

Environment

STD300

Cause

Internal hardware upgrade that does not affect the functionality. 

Resolution

The USB port is in place for internal/factory use only, and should not be used in the field.