How do I reset the Windows password on a Pelco DVR/HVR?

Issue

How do I reset the Windows password

Product Line

Pelco Video Management

Environment

  • DX8000
  • DX8100
  • DS SRV
  • DSSRV2
  • DS Xpress
  • DS RealVue Xpress
  • DS1000

Cause

  • Unable to login to Windows
  • Forgot the Windows password

Resolution

In order to reset the Windows password on a Pelco DVR/HVR an OS Recovery will need to be performed

Related topics: How do I run system Recovery on a DX8000 Series DVR/HVR?

Related topics: How do I run System Recovery on a DX8100 Series DVR/HVR?

Related topics: How to perform a recovery on the DSSRV series Network Video Recorder

Related topics: Perform an operating system (OS) recovery on a Digital Sentry system