DX8100HDDI Event Messages List.

Issue

DX8100HDDI Event Messages List.

Product Line

Pelco Video Management

Environment

  • DX8100HDDI

Cause

  • Hardware failure on a DX8100HDDI

Resolution

The controller events can be categorized as follows according to the severity levels:

  • Critical: Errors that need to attend to immediately.
  • Warning: Errors.
  • Notification: Command processed message sent from Firmware.

The RAID subsystem records all system events from power on, it can record up to 1,000 events. To power off or to reset the controller will cause an automatic deletion of all the recorded event logs.

Refer to SCSI to SATA RAID Subsystems Operation Manual for event message list.Click here to download. (Appendix C)

Related Articles:

How do you log into a DX8100HDDI?